Technical FAQs

Ask a Question

Where can I find the part numbers and pricing for the Automation support program?

The Automation Support Program allows the customer to have priority telephone support as well as keep their software up to date.  There are 2 brochures attached to this FAQ.  The Automation Support Pricing Brochure has a grid that will provide the part number and pricing based on the type of software platforms you have as well as the number of licenses. The Automation Support Brochure explains the different levels of support that we provide at the Andover, MA Technical Support Center.  If you still have questions don't hesitate to contact the Contract Support Group at 888-266-8705 option 3.
Was this helpful?
What can we do to improve the information ?