Technical FAQs

Ask a Question

Where would you refer customers seeking warranty information on Industrial Automation products?

Issue: Warranty information


Product Line: Industrial Automation products


Environment: None

Cause:

Resolution:

Warranty inquires on Industrial Automation products should be directed to Schneider Electric's Industrial repair Center.
They can be reached by dialing 1-800-950-9550, option 3 for customer service (or) by dialing 1-800-468-5342 - Option 2 for Customer service.
They can also be contacted via email at industrialrepair@schneider-electric.com

The address for the repair center is

Schneider Electric
Attn: Repair
235 Burgess Rd
Greensboro NC 27409 

Note: There is no internal five digit dial.

Was this helpful?
What can we do to improve the information ?