Technical FAQs

Ask a Question

What are the dimensions of the HMIZSURDP unit?

  Title

What are the dimensions of the HMIZSURDP unit?

Issue

Customers that are looking for the dimensions of the HMIZSURDP.

Product Line

Magelis HMISCU

Environment


 

Cause

Resolution

Below are the dimensions of the HMIZSURDP unit.  Also attached is the PDF file.

Was this helpful?
What can we do to improve the information ?