Technical FAQs

Ask a Question

Why can't an Advantys STB AC input module be selected as a Reflex Action input ?

The AC input modules (STBDAI5230, STBDAI5260 and STBDAI7220) do not have a module status bit used by the Reflex action to determine the health of the module as well as the health of the input signal.
Was this helpful?
What can we do to improve the information ?