Technical FAQs

Ask a Question

Can the fast outputs FQ0 and FQ1 on the HMISCU controllers be used as regular outputs?

Yes, The outputs on the HMISCU controllers by default are regular outputs. Output FQ0 and FQ1 can be configured as PTO or PWM.
Was this helpful?
What can we do to improve the information ?