Technical FAQs

Ask a Question

What would cause an "ERR" light to flash on an Advantys Analog I/O card?

The ERR light on an Advantys Analog I/O module will flash if any of the channels are unused. When the Island is configured by default the I/O channels on the analog cards are all enabled. To resolve the error you  will need to edit the module configuration using the  Advantys configuration software. Open the module and under channel configuration disable all of the unused channels and download the new configuration  to the NIM. This will clear the error on the analog cards. 
Was this helpful?
What can we do to improve the information ?