Technical FAQs

Ask a Question

Where do I place my 'Help on Type' file when creating a custom DFB in Unity Pro v7.0?

When using Unity Pro v7, the Tools - Options - Custom Library path should be set to the following:
      c:\Program Data\Schneider Electric\Unity Pro\CustomLibset\V7.0.

The associated .htm Help file should be placed in:
      c:\Program Data\Schneider Electric\UnityPro\CustomLibset\V7.0\CustomLib\MyCustomFam\ENG

Was this helpful?
What can we do to improve the information ?