Technical FAQs

Ask a Question

Can the state of Twido discrete inputs be moved into a memory word?

Title

Can the state of  Twido discrete inputs be moved into a memory word?
 

Issue

The customer wants to send the state of the inputs in a Modbus message..

Product Line

Twido PLC and Twido Suite

Environment

Twido Suite 2.31.04

Cause

Resolution

Insert an Operate Block into the program. The expression, %MW100:=%I0.0:16, will move the state of inputs 0-15 into memory word 100. Note: the starting address of the Inputs must be a multipal of 16.

 

Was this helpful?
What can we do to improve the information ?