Technical FAQs

Ask a Question

Can I connect to both ports on a Quantum 140NOE771xx at the same time and receive data from each?

Issue:
Can I connect to both ports on a Quantum 140NOE771xx at the same time and receive data from each?


Product Line:
Quantum 140NOE771xx


Environment:
N/A


Cause:
N/A


Resolution:
No, the 140NOE771xx is a one channel device. It is capable of communicating over either a 10/100BASE-T or a 100BASE-FX Ethernet network at any given time, but not over both at the same time.

 

 

Was this helpful?
What can we do to improve the information ?