Technical FAQs

Ask a Question

How can I join 3 variables to one object without using scripting, in Vijeo Designer?

You can join the 3 variables using a string display object and in the expression editor using the following syntax: Tag1 + Tag2 + Tag3

Where Tag1, Tag2, Tag3 are variable names.
If you want spacing between the values being displayed, then you will need to add " " between each tag.  For example: Tag1 + " " + Tag2 + " " + Tag3

This will work with any data type variables (integer, real, string).  But keep in mind that if you use this feature, you will not have input mode.
Was this helpful?
What can we do to improve the information ?