Technical FAQs

Ask a Question

Designer Error: Designer cannot contact the tree manager on the station

Issue
When a user attempts to open an ION meter template, the Query Server or the Log Inserter in Designer the following errors occur:

the communications server is not responding to tree request on .
-- the communications server on. should be restarted


                   

designer cannot contact the tree manager on the station:
.
please fix the problem and try again


                   


In Task Manager, validate.exe *32 and treemon.exe *32 processes would terminate shortly after a meter template was opening in Designer.

The following error is in Windows Event Viewer:
    Log Name: Application 
    Source: Application Error 
    Date: 2/21/2014 1:18:54 PM 
    Event ID: 1000 
    Task Category: Application Crashing Events 
    Level: Error 
    Keywords: Classic 
    User: N/A 
    Computer: CNPEGASYS 
    Description: 
    Faulting application name: awrem32.exe, version: 12.1.0.446, time stamp: 0x464443dd 
    Faulting module name: ntdll.dll, version: 6.1.7601.17514, time stamp: 0x4ce7ba58 
    Exception code: 0xc0150010 
    Fault offset: 0x0008477b 
    Faulting process id: 0x192c 
    Faulting application start time: 0x01cf2f39b03c1fb3 
    Faulting application path: D:\Program Files (x86)\Symantec\pcAnywhere\awrem32.exe 
    Faulting module path: C:\Windows\SysWOW64\ntdll.dll 
    Report Id: 006e35a9-9b2d-11e3-bbc6-782bcb3411f6

Product Line
ION Enterprise 6.0
SPM 7
PME 7.2

Environment
Designer

Cause
The causes of ntdll.dll error messages can vary greatly. However, most ntdll.dll errors result from a corrupt or damaged version of the ntdll.dll file itself, corrupt hardware drivers, or issues between Windows and other programs.  Third party software programs that have been installed on your computer are almost always the cause of ntdll.dll errors.

More information can be found here:
     http://pcsupport.about.com/od/fixtheproblem/a/ntdlldll.htm

In the above case PCAnywhere was installed.

Resolution
Install most recent operating system service pack and updates.
If third party software program has any updates or service packs available, install them too.
 

Was this helpful?
What can we do to improve the information ?