Technical FAQs

Ask a Question

Unable to enable Maintenance Mode in Event Notification Manager (ENM) on Windows Server 2008

Issue:
Unable to enable Maintenance Mode in ENM on Windows Server 2008. After clicking the check box the system prompts for a reason, which is then entered, then clicking continue does nothing.

Product Line:
APM 6.4, ENM 7.0, ENM 7.1

Cause:
Internet Explorer Enhanced Security Configuration (IE ESC)is enabled

Resolution:
Disable Internet Explorer Enhanced Security Configuration
1. Open the Server Manager Tool. Configure IE ESC is located on the right hand side of the interface in the section heading Security Information.
2. Select the link Configure IE Esc and the configuration window will open.
3. Open Internet Explorer and notice the glaring Warnings that IE ESC has been disabled. 
4. You may change the Local Intranet Zone settings or request not to have the message displayed in the future. 
Was this helpful?
What can we do to improve the information ?