Technical FAQs

Ask a Question

VAMP 321 arc flash sensors no longer function after connecting a VAMP 10L module

Issue:
After connecting a VAMP 10L module to the VAMP 321 relay the VAMP 321 arc flash sensors no longer trigger a trip.

Product Line:
VAMP 321

Resolution:
This issue may be caused by connecting the VAMP 10L module to the VAMP 321 incorrectly. Verify that the communication port on the VAMP 321 matches that on the VAMP 10L. If they do not match correct this then reconfigure the connection under the ARC Protection screen within VAMPset and write these changes to the VAMP 321. Finally confirm functionality.
Was this helpful?
What can we do to improve the information ?