Technical FAQs

Ask a Question

What do the green lights on the VAMP 10L module indicate

Issue:
There are solid green lights on the VAMP 10L module, what do these indicate?

Product Line:
VAMP 321, VAMP 221

Resolution:
The solid green lights indicate that the attached arc flash sensor is connected and is functioning properly. If the light is not illuminated this indicates an issue with the wiring to the arc flash sensor or an issue with the sensor itself.
Was this helpful?
What can we do to improve the information ?