Technical FAQs

Ask a Question

Is the memory or SIM card required for Advantys STB?

No, the removable memory card is optional since the NIMs have flash memory.  When the configuration software is not used and the system is auto-configured, the configuration is saved to flash only.  To use the removable SIM card, the configuration software is required and an action to Save to the SIM card has to be performed while online.
Was this helpful?
What can we do to improve the information ?