Technical FAQs

Ask a Question

What are the different File Formats for Symate Plus?

What are the different File Formats for Symate Plus?

There are 3 different File Formats for Symate Plus. They are:

SP2 = Symate Plus version 2
SP1 = Symate Plus version 1
SFW = Symate SFW3XX

Note: Symax software will only run on software up to Windows XP and the software and product line was obsoleted in 2013 and it would be recommended to upgrad to the M580 product line.

The SFW that you have and the version of the software will determine what File Formats are available.

SFW 472 Symate Plus, Version 2 only, contains the option of selecting all 3 File Formats, SP1, SP2 and SFW. With this you can take programs and go between the different versions of software changing the file format to work in any version of software.

The formats are as follows:

 
File Format
   
File Extension
   
SP2
.RNG
.REG
.LAB
.HDR
.TTL
SP1
.PRG
.LAB
.HDR
.TTL
 
SFW
.RNG
.REG
.LBL
   
  • .RNG = Rungs
  • .LAB = Labels
  • .TTL = Title
  • .REG = Registers
  • .LBL = Labels
  • .PRG = Program
  • .HDR = Headers
Was this helpful?
What can we do to improve the information ?