Technical FAQs

Ask a Question

What does BATL displayed on the Unity Quantum LCD panel indicate?

This would indicate that the battery is either low in voltage or disconnected altogether. The front LCD panel cover slides straight up vertically from the silk screened triangle to expose the battery.
Was this helpful?
What can we do to improve the information ?