Technical FAQs

Ask a Question

What could cause a MSTR error 6101 over Ethernet?

The error 6101 error is a routing error. This is usually caused by the Head # and Map Index is set wrong. e.g. if you NOE card is in slot 3 and you are not going through a bridge the it will be set to 300 hex and not 3. This has to do with high byte low byte and the head number is in the high byte.
Was this helpful?
What can we do to improve the information ?