Technical FAQs

Ask a Question

What is the I/O map register assignment for the 140DSI35300?

The 140DSI35300 is I/O mapped as 64 discrete inputs or 4 input words.  The first 32 discrete inputs or 2 words represents the actual discrete inputs of the module.  The next 32 discrete inputs or 2 words represents the broken wire status of each input.
Was this helpful?
What can we do to improve the information ?