Technical FAQs

Ask a Question

What cable is needed for a Micrologix 1200 to a Magelis HMISTO511?

The cable is XBTZ9733. It has a RJ45 on the Magelis side and an Mini din on the other end, it will support either RS232 or RS485.
Was this helpful?
What can we do to improve the information ?