Technical FAQs

Ask a Question

How many Unity Pro MBP_MSTR Blocks can run at one time over Etherent using a 140NOE77101 module?

The limitation is 16. Should you program more than 16 without sequencing, the PLC will only process 16 at a time and progress through the others as the blocks complete.
Was this helpful?
What can we do to improve the information ?