Technical FAQs

Ask a Question

Can I have a mix of devices on the same Modbus Plus network that contains a Momentum Cluster Mode cabling scheme?

Yes. A Modbus Plus network may consist of a mixture of devices so long as the user understands the following 

  • Only TSX Momentum devices may be used within the Cluster.
  • The MB+ segment will be limited to 32 node devices per 1500' segment.
  • MB+ cable segments must be connected by an RR85 Repeater.
  • A maximum of 3 Repeaters may be used with up to 4 network segments.

Was this helpful?
What can we do to improve the information ?