Technical FAQs

Ask a Question

How do I mount the CM4XXX series Base?

Issue
Mounting the CM4XXX series base

Product Line
CM4000
CM4250
CM4000T

Environment
Installation

Cause 
The best method of installation for safety and product longevity

Resolution
There are 2 methods to mount the CM4000 properly:
(1) Mount the CM4000 on a vertical pan with the control power at the top, or;
(2) Mount the CM4000 on the floor of the compartment.

Any other method may cause the unit to over heat at 70 degrees C. Please refer to pages 15 and 16 of the CM4000 Installation Manual.

 

Was this helpful?
What can we do to improve the information ?