Technical FAQs

Ask a Question

Message Queing installation fails with Error Code: 0x42C. Error Description: The dependency service or group failed to start

The service NT LM Security Support Providor must be running in order to install Microsoft Message Queuing (MSMQ)


  • 1. Click on the Windows START button
    2. Select Run
    3. Type in services.msc - This will open the services console
    4. Enable the service "NT LM Security Support Provider" by right clicking and go to properties. Set the Start up mode to Manual mode, click OK
    5. Install MSMQ again

Legacy KB System (APS) Data: RESL204824 V1.0, Originally authored by MaTh on 03/16/2011, Last Edited by MaTh on 03/16/2011
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0, SMS Add-on
Was this helpful?
What can we do to improve the information ?