Technical FAQs

Ask a Question

How to turn off User Access Control (UAC) in Windows Server 2008

Goals and Symptoms

Summary
It may be necessary to disable User Access Control in Windows Server 2008 before being able to install PowerLogic software.

Causes and Fixes

Procedure

Turning off user access control (Windows 2008)

To turn off user access control:


  • 1. Click Start > Administrative Tools > System Configuration
    2. On the Tools page, scroll down and select Disable UAC/Disable User Access Control (requires reboot).
    3. Click Launch, and then close the command prompt window.
    4. Click OK, and then reboot the server.

Legacy KB System (APS) Data: RESL203938 V1.0, Originally authored by MaTh on 11/19/2010, Last Edited by MaTh on 11/19/2010
Related ranges: System Manager 4.3, ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?