Technical FAQs

Ask a Question

Can the Min/Max/Avg Log of a Circuit Monitor be added to an upload task in System Manager Software (SMS)?

The Min/Max/Avg Log is an onboard log that is present by default under Onboard Files for CM3000 series and CM4000 series meters. This log can only be viewed manually by going to Display and selecting On-Board Data File in System Manager Software Setup Utility. The Min/Max/Avg Log stores interval minimum, maximum, and average data from the circuit monitor. This data is not logged to the SMS database.


  • In order to log the minimum, maximum, and average values for various parameters and upload them as scheduled tasks, you must add each min/max/avg quantity into a pre-existing or new log template. The log template can then be assigned to an onboard data file in the meter and logged/uploaded like any other data log.

Legacy KB System (APS) Data: RESL199623 V1.0, Originally authored by MaTh on 08/14/2009, Last Edited by MaTh on 08/14/2009
Related ranges: CM4000 series, CM3000 series
Was this helpful?
What can we do to improve the information ?