Technical FAQs

Ask a Question

Does ION Enterprise 5.6 support Windows XP Embedded ?

Windows XP Embedded (XPE) is a subset of Windows XP. Developers use Windows Embedded to take advantage of the ability to run thousands of existing Windows applications and drivers on a variety of smart, connected, and service-oriented advanced commercial or consumer devices. At this time, no versions of ION Enterprise are supportedt on it.



  • Date Created: 27 Mar 2009
    Original Author: JC
    Public
    All content © 1992-2009 Schneider Electric

Legacy KB System (APS) Data: RESL198180 V1.0, Originally authored by KBAdPM on 04/01/2009, Last Edited by KBAdPM on 04/01/2009
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?