Technical FAQs

Ask a Question

Does Advanced Reports (AR) have to be installed before Upgrading to System Manager Software (SMS) version 4.2?

Advanced Reports (AR) does not have to be installed previous to upgrading SMS version 4.2.
From page 34 of the System Manager Software Setup Guide Version 4.2, step 23 states:
"If no previous Advanced Reports software is installed on this computer, a message displays telling that it will be installed. This will install Crystal Enterprise and then the SMS Advanced Reports software."


  • Date Created: May 19, 2008
    Last Revised: June 24, 2008
    Public
    Original Author: AV
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL192204 V1.0, Originally authored by PhHa on 06/25/2008, Last Edited by PhHa on 06/25/2008
Related ranges: SMS Add-on, System Manager 4.0
Was this helpful?
What can we do to improve the information ?