Technical FAQs

Ask a Question

Error during install of SMS 3.3 : "Error 1920. Service Sentinel (Sentinel) failed to start"

Goals and Symptoms

The following error message is shown when installing SMS V3.3 on a PC with Win XP Service Pack 1 or higher.
.


ERROR MESSAGE TEXT
========================
Sentinel System Drive Installer Information
-----------------------------------------------------------
Error 1920. Service Sentinel (Sentinel) failed to start. Verify that you have sufficient privileges to start system services.
========================

Causes and Fixes

Windows 2003 SP1 and Windows XP SP2 introduce a new technology called Data Execution Prevention (DEP). The installation fails because DEP detects and prevents each service from installing or starting.

Complete one of the following steps:

Disable DEP for all services and programs other than those needed by Windows as follows:

1. Go to Control Panel > System > Advanced.
2. Click the 'Settings' button in the 'Performance' area and then click the 'Data Execution Prevention' tab.
3. Click 'Turn on DEP for essential Windows programs and services only'.
4. Click 'OK'.
5. Restart your computer for changes to take effect.
6. Install sentinel.

- OR -

Disable DEP for all Windows services, processes, and applications as follows:

1. Open the Boot.ini file in the Windows root directory.
2. Search for "/noexecute=" and change it to "/noexecute=AlwaysOff".
3. Restart your computer for changes to take effect.
4. Install sentinel.

  • Last Revised: 5th June 2008

    Applies To: Installation of System Manager Software V3.3

    Original Author: EC

    Public

    All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL192077 V1.0, Originally authored by KBAdPM on 06/05/2008, Last Edited by KBAdPM on 06/05/2008
Related ranges: System Manager 3.3
Was this helpful?
What can we do to improve the information ?