Technical FAQs

Ask a Question

What are the part numbers for the different Input / Output Extender (IOX) modules? Which color corresponds to each type of module (digital, analog, input, output)?

See the following table for the different colors and part numbers of IOX modules and what they represent.


The IOX modules are as follows:
IOX0404 = 4 digital inputs and 4 digital outputs
IOX2411 = 4 digtial inputs (DC), 2 digital outputs (DC), 1 analog input, and 1 analog output
IOX08 = 8 digital inputs (DI120AC)
IOX = blank I/O extender module with a maximum of 4 analog outputs.


  • Date Created: April 16, 2008
    Last Revised: September 5, 2012
    Public
    Original Author: AV
    All content © 1992-2012 Schneider Electric
Was this helpful?
What can we do to improve the information ?