Technical FAQs

Ask a Question

What does Scale Factor I, V, W, and E represent in the Series 200 and 700 Power Meter (PM200, PM700) Register List?

The Series 200 and 700 Power Meter variables (I, V, W, and E) correspond to the scale factors of the current (4105), voltage (4106), power (4107), and energy (4108) quantities respectively. The scale factor register values represents the power of 10.



  • Date Created: April 11, 2008
    Last Revised: May 23, 2008
    Public
    Original Author: DB
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL192008 V1.0, Originally authored by PhHa on 05/24/2008, Last Edited by PhHa on 05/24/2008
Related ranges: PM200 series, PM700 series
Was this helpful?
What can we do to improve the information ?