Technical FAQs

Ask a Question

Would ME kilowatt hour meter roll back to 0 after reaching maximum display capacity 9999 kWh?

After 9999.99 kWh, the counter will switch to 10.000 MWh. It will continue until it reaches 99999 MWh.
At this point, you must reset your "partial" counter, in order fo the recordings to continue.
The "total" counter cannot be reset and will remain at 99999 MWh unless the meter is sent back to the factory for a total energy reset.

Keywords and Phrases:

rollover value, maximum range, capacity, display range, counter range, exceed, maxed out, display limitation, precision

  • Last Revised: 22 May 2008

    Applies To: ME energy meter

    Original Author: EC

    Public

    All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191989 V1.0, Originally authored by KBAdPM on 05/22/2008, Last Edited by KBAdPM on 05/22/2008
Related ranges: ME
Was this helpful?
What can we do to improve the information ?