Technical FAQs

Ask a Question

WAGESD10 Meter Instruction Bulletin, 3070IB0702

This Add-on is supported in System Manager Software v 3.3.2.3 and 4.x. All reports require Information Manager.
See attachment:

WAGES_D10_IB.pdf




  • Date Created: April 4, 2008
    Last Revised: May 8, 2008
    Public
    Original Author: RM
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL191863 V1.0, Originally authored by PhHa on 05/09/2008, Last Edited by PhHa on 05/09/2008
Related ranges: SMS Add-on, PowerLogic Enclosure - WAGES
Was this helpful?
What can we do to improve the information ?