Technical FAQs

Ask a Question

What happened to Enterprise Manager in SQL2005 of System Manager Software (SMS)?

Enterprise Manager is a SQL2000 database interface that allows viewing and configuration of SQL databases. It installs when SQL2000 is installed. It is not available with MSDE2000.
Enterprise Manager was replaced by SQL Server Management Studio in SQL2005. It installs with SQL2005. For MSDE2005 the SQL Server Management Studio Express can be downloaded free and gives most of the functionality as the Studio version. Here is the link: http://www.microsoft.com/downloads/details.aspx?FamilyID=c243a5ae-4bd1-4e3d-94b8-5a0f62bf7796&displaylang=en

SMS version 4.0x:
System Manager Software Professional (SMSPE) version 4.0x uses SQL 2000 databases (no size limit).
System Manager Software Standard Edition (SMSSE) and Device Limited (SMSDL) uses MSDE 2000 databases (2 gig limit).

SMS version 4.2 and later
System Manager Software Professional (SMSPE) uses SQL 2005 databases (no size limit).
System Manager Software Standard Edition (SMSSE) and Device Limited (SMSDL) uses MSDE 2005 databases (2 gig limit). SQL Server Management Studio Express can be manually downloaded.


  • Date Created: March 7, 2008
    Last Revised: April 29, 2008
    Public
    Original Author: MT
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL191803 V1.0, Originally authored by PhHa on 04/30/2008, Last Edited by PhHa on 04/30/2008
Related ranges: System Manager 4.0
Was this helpful?
What can we do to improve the information ?