Technical FAQs

Ask a Question

How to configure System Manager Software (SMS) to auto-upload waveform captures from Sepam Relays Series 20, 40 and 80?

Goals and Symptoms

How to configure System Manager Software (SMS) to auto-upload waveform captures from Sepam Relays Series 20, 40 and 80?

Facts and Changes

This applies to System Manager Software (SMS) version 4.x

Causes and Fixes

Follow the steps below to configure SMS to Auto-upload waveform captures from Sepam relays Series 20, 40 and 80:
1. In SMS click on "Setup" -> "Scheduled Tasks"

2. Click on "Tasks" and then click on "add"
3. Create a Task Name and choose "onboard datalog/ waveform upload" for Task Type
4. Click on "continue"

5. Select the Device Type and Device
6. Move Extended WFC from Available Files to Selected Files and click "ok"
7. Click "close" and save changes

8. In "Setup Scheduled Task" menu click "add" and enter a Reference Time and Interval

9. Click "ok" and highlight the reference Time
10. Move the task from Tasks Available to Task Selected

11. Click "close" and save changes


 

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7e8545de0017b7eac125741800165be6/fl_block_5/0.1AD6?OpenElement&FieldElemFormat=gif)

  • Date Created: February 22, 2008
    Last Revised: March 25, 2008
    Public
    Original Author: JJ
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL191511 V1.0, Originally authored by PhHa on 03/26/2008, Last Edited by PhHa on 03/26/2008
Related ranges: System Manager 4.0
Was this helpful?
What can we do to improve the information ?