Technical FAQs

Ask a Question

Are waveform captures dependant on the System Manager Software (SMS) system they were uploaded to?

Each waveform capture that is uploaded by a SMS task or exported manually is associated to the System ID and Device ID in the database. The system that is placed on-line in SMS is the one that has the active view. This is what filters the view of the waveforms in the web pages and in the SMS setup utility (Display>waveform plots>select the device). It is possible to view waveforms from other devices associated to another system through the SMS setup utility by selecting Display>Waveform plots>Import waveforms>then browse to the folder where the uploaded files are located.
Applies to all versions of System Manager Sofware, SMS


  • Original article#
    Date Created: January 10, 2008
    Last Revised: February 5, 2008
    Public
    Original Author: MN
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL190991 V1.0, Originally authored by PhHa on 02/06/2008, Last Edited by PhHa on 02/06/2008
Related ranges: System Manager 3.3, System Manager 4.0
Was this helpful?
What can we do to improve the information ?