Technical FAQs

Ask a Question

Why devices do not show up in billing after installation of Tenant Metering Software - Commercial Edition (TMSCE) version 2.0 .

Tenant Metering Software - Commercial Edition, TMSCE software must collect a day's worth of data before the devices will appear for billing. Wait a day after setup to allow this data to come into the database and the meters should appear in the billing.



  • Original article#
    Date Created: December 19, 2007
    Last Revised: February 5, 2008
    Public
    Original Author: MN
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL190983 V1.0, Originally authored by PhHa on 02/05/2008, Last Edited by PhHa on 02/05/2008
Related ranges: Tenant Metering Software
Was this helpful?
What can we do to improve the information ?