Technical FAQs

Ask a Question

How to configure color banding on Meters in System Manager Software (SMS)

How to setup color banding on Display > Meters in SMS.


Resolution

This is done by configuring Functions/Alarms. A Function/Alarm must be setup on each device for each quantity to use the feature.

See below instructions on setting this up.

In SMS go to Setup > Functions/Alarms

Select the device for setting up the alarm and it will show the Functions Available

Move the Function you want the banding for over to Functions Selected

Setpoints will then become available for that Function

Click the Setpoints button and you will see the following screen.

The Pickup value represents the upper band limit and the Dropout represents the lower limit of the band.

The condition represents the band range that will be displayed.

**Note: In order for the banding to take effect at least two Conditions and Pickup and Dropout have to be setup.

 


  • Original article#
    Date Created: August 14, 2007
    Last Revised: January 29, 2008
    Public
    Original Author: KT
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL190870 V1.0, Originally authored by PhHa on 01/30/2008, Last Edited by PhHa on 01/30/2008
Related ranges: System Manager 4.0, System Manager 3.3
Was this helpful?
What can we do to improve the information ?