Technical FAQs

Ask a Question

Can Information Manager Reports be stored in a different folder location or disk drive?

Goals and Symptoms

Issue
Customer want to change the location where IM reports are stored.

Causes and Fixes

Resolution
 

In order to select a different folder location for Information Manager to store reports, navigate to File>Change Report Folder within Information Manager and select the appropriate folder. Similarly, the user could select the Change Report Folder icon on the toolbar.

Note: When making a change to the Report Folder within Information Manager, the old reports and report configuration files do not move to the new report folder location automatically. It may appear as if all of the old reports and report configurations are missing but they will still be in the original reports folder (For SMS 4.0 and greater, POWERLOGIC\InfoManager\Reports is the default folder).


Legacy KB System (APS) Data: RESL189626 V2.0, Originally authored by KBAdPM on 11/24/2007, Last Edited by MaTh on 01/07/2013
Related ranges: System Manager 4.0, System Manager 3.3
Was this helpful?
What can we do to improve the information ?