Technical FAQs

Ask a Question

Confusion about upgrading 7700 meter firmware (what "older cards" means)

Goals and Symptoms

On support website to upgrade the firmware of the ION7700 meter, it mentions that older cards should be upgraded through COM 2. This is a bit confusing as it is unclear what is meant by the term "older" in this context.

Facts and Changes

7700
Firmware upgrade old

Causes and Fixes

If the firmware version on the 7700 meter is older than V135 the upgrade should be done using the COM2. Anything after 7700 should be OK to upgrade using either COM port.

  • Original article#12725

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188801 V1.0, Originally authored by KBAdPM on 11/03/2007, Last Edited by KBAdPM on 11/03/2007
Related ranges: ION7700
Was this helpful?
What can we do to improve the information ?