Technical FAQs

Ask a Question

ION Setup Installation Error "Can’t run 16-bit Windows Program ..."

Goals and Symptoms

Summary


  • An error message is displayed when trying to install ION Setup.


    Cant run 16-bit Windows Program
    Cannot find file C:\DOCUME~1\u444253\Local Settings\Temp\2\pft6B.tmp\Setup.exe (or one of its components).
    Check to ensure the path and filename are correct and that all required libraries are available.
     

    Symptoms
    The error message above is displayed when the installer is first run after downloading ionsetup.exe from
    http://www.pwrm.com/PRODUCTS/IONSetup/

Facts and Changes

Keywords
Installation
Winzip
Zip

Causes and Fixes

Cause
The ION Setup installer runs in two stages to successfully install ION Setup. First, ionsetup.exe is self extracted using Winzip into a temporary location (%USERPROFILE%\Local Settings/Temp). Second, the setup.exe file is run to install the actual program.

The first step will fail if the version of Winzip used is not compatible the operating system. This is more likely to happen using an XP version of Winzip on Windows Server 2003.

The error message is displayed once the ionsetup.exe program is launched since the self-extraction failed in the first step.
 

Resolution
Install the correct version of WinZip.

Another error can occur if the files are manually extracted without using the correct version of WinZip:



WinZip 6.3-8.0
WinZip 6.3-8.0 has a known compatibility issue with this version of Windows. For an update that is compatible with this version of Window, contact Nico Mak Computing
To run the program, click Continue. For more information, click details.

Select Continue to get ionsetup.exe extracted. The installer will likely run now, but if it does not download the correct version of WinZip.

More Information
http://www.winzip.com/prod_down.htm



Last Revised: September 17, 2007

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188150 V1.0, Originally authored by KBAdPM on 09/20/2007, Last Edited by KBAdPM on 09/20/2007
Related ranges: ION Setup 2.1
Was this helpful?
What can we do to improve the information ?