Technical FAQs

Ask a Question

What components make up a MCTAS485 or a MCT485 terminator?

MCT485 = Multi Communcations Terminator for RS485 connections (has spade lug connectors)

  • MCTAS485 = Multi Communcations Terminator for PowerLink AS panels for RS485 connections (has tinned wire terminals)
  •  
  • Both terminators contain a 100 ohm, .25 watt resistor in series with a .047uf capacitor. There are 2 sets required for a each MCT connection. One set should be connected across the RX+ and RX- and one across the TX+ and TX-.
  •  
  • See attached internal wiring diagram of the MCTAS485. The wiring diagram is the same for the MCT485.
  •  
  • MCTAS485 Internal Diagram-Dimensions.pdf
    • Original article# 4701

      Last Revised: September 13, 2007

      Public

      All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188076 V1.0, Originally authored by PhHa on 09/13/2007, Last Edited by PhHa on 09/13/2007
Related ranges: Communication Wiring for Power Management Systems
Was this helpful?
What can we do to improve the information ?