Technical FAQs

Ask a Question

System Manager Software Admin Utility hangs after putting in the Password and clicking Apply.

This can sometimes occur when currently logged into the server using a Domain account. Log-off Windows with the Domain account and log back in using a local administrator account. Then try running the Admin Utility.
Environment:
System Manager Software v 3.3 or v 4.0

  • Last Revised: September 9, 2007

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL187981 V1.0, Originally authored by PhHa on 09/10/2007, Last Edited by PhHa on 09/10/2007
Related ranges: System Manager 3.3, System Manager 4.0
Was this helpful?
What can we do to improve the information ?