Technical FAQs

Ask a Question

Can the Active Pager Module send pages to a third party interface.

The Active Page Module (APM) software uses SMTP protocol to send email pages and/or a modem connection to send pages to alphanumeric pagers. These are the only two methods supported and tested.


  • Last Revised: September 5, 2007

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL187906 V1.0, Originally authored by PhHa on 09/06/2007, Last Edited by PhHa on 09/06/2007
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?