Technical FAQs

Ask a Question

Error occurs when adding a Custom Quantity to a log template in System Manager Software (SMS). SMSSetupUtil Error: “Unable to add the quantity because it will exceed the maximum allowable number of registers which is 97.”

Goals and Symptoms

Error occurs when adding a Custom Quantity to a log template in SMS. SMSSetupUtil Error: Unable to add the quantity because it will exceed the maximum allowable number of registers which is 97.


Causes and Fixes

This error occurs because the Powerlogic Network Server was not restarted after creating a new Custom Quantity. Follow the steps below to correct the error.

  1. Close the SMS Setup Utility.
  2. Restart the Powerlogic Network Server (the PowerLogic Network Server may be running as a service)
  3. Open the SMS Setup Utility and verify that the Custom Quantity can be added to the Log Template.

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/dd8dc7f3e02233c4c125733f0016257b/fl_block_5/0.1AD6?OpenElement&FieldElemFormat=gif)Last Revised: 12 August 2007

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL187513 V2.0, Originally authored by PhHa on 08/13/2007, Last Edited by KBAdPM on 08/22/2007
Related ranges: System Manager 4.0, System Manager 3.3
Was this helpful?
What can we do to improve the information ?