Technical FAQs

Ask a Question

Is System Manager Software (SMS) v 4.0 compatible with Windows Vista?

SMS version 4.0, v 4.0 SU2, and v 4.2 are not supported on a Windows Vista operating system. It can be installed on Windows XP, 2000 and 2003 operating systems. See the SMS 4.0 computer specifications below for more information.

  • Last Revised: 5 August 2007

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL187409 V2.0, Originally authored by PhHa on 08/06/2007, Last Edited by KBAdPM on 09/13/2007
Related ranges: System Manager 4.0
Was this helpful?
What can we do to improve the information ?