Technical FAQs

Ask a Question

System Manager Software (SMS) v4.0 Error: “Invalid file version, table not opened” when opening a SMS table.

The table may be corrupt. Try replacing the "table name".PLTable with a known working copy from a computer with the same version of SMS.


  • Last Revised: 3 August 2007

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL187391 V2.0, Originally authored by PhHa on 08/03/2007, Last Edited by KBAdPM on 08/22/2007
Related ranges: System Manager 4.0
Was this helpful?
What can we do to improve the information ?