Technical FAQs

Ask a Question

PMCU (Powerlogic Meter Configuration Utility) software download location with Optional Viewing Features

Issue
PMCU includes an optional feature called Viewing Features. User needs to know where to find the installer and how to activate the Powerlogic Meter Configuration Utility (PMCU) with optional viewing features.
 

Product Line
Powerlogic Meter Configuration Utility (PMCU v2.11)

Environment
Viewing Features includes:
View real-time data in quick tables
View waveforms
View on-board data files
View PowerLogic meter configuration reports
Check device status
Perform device registry read and write commands

Cause
PMCU includes an optional feature called Viewing Features which needs to be manually activated if the latest version of PMCU is not installed (v2.11). 
ION Setup will not access onboard waveform data on Powerlogic Meters including the CM2000, CM3000, CM4000, and PM800 series of meters.
NOTE: In order to have the CM2000 as an available device you must first locate the driver via this directory path C:\POWERLOGIC\PMCU\OptionalInstalls, and double-click on the driver once you've closed PMCU

Resolution
The new version (v2.11) of the PMCU software does not require this extra activation as the features are included by default. The latest version of PMCU (v 2.11) can be downloaded from link below:
PMCU v2.11 

NOTE: In order to install PMCU on Windows 7, please follow KB FA293363
 
Was this helpful?
What can we do to improve the information ?