Technical FAQs

Ask a Question

System Manager Software (SMS) device type install error: “Unable to communicate with COMPUTERNAME\SMS3000. Verify that you can access the Server and that SQL is started.”

The MSSQL System Administrator (sa) account password has been changed from the default. Click OK, then enter the current sa account password in the next dialog box and the install will proceed.


  • Last Revised: 3 August 2007

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL187388 V2.0, Originally authored by PhHa on 08/03/2007, Last Edited by KBAdPM on 09/13/2007
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?