Technical FAQs

Ask a Question

Logging data with the PM210 Device type in the Ethernet Gateway EGX400.

The Series 200 Power Meter (PM210) is not a loggable device type in the EGX400 with firmware v 5.6. A device type template (.plt) file will be created at a later date. A temporarily work around is to select the PM700 device type for the PM200 meter and then enable logging. The PM700 and the PM200 share some of the same registers. Some PM700 quantities may not be applicable for the PM200.


  • Last Revised: 17/7/2007

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL187130 V2.0, Originally authored by PhHa on 07/17/2007, Last Edited by KBAdPM on 04/01/2009
Related ranges: PM200 series, EGX400
Was this helpful?
What can we do to improve the information ?